DRDY引脚在START引脚拉高之前就一直是3.3v的高电平,请问这正常吗?
AVDD=2.5V,AVSS=-2.5V,DVDD=3.3V。
其中VCAP1=-1.3V,VCAP2 = 0V,VCAP3 = 1.67V。
想采用内部参考,但是不能写入寄存器,不能将PD_REFBUF置为1。所以VREFP=VREFN= -2.5V。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
板子是您自己做的,还是TI的评估板?
VCAP电压是参考AVSS的电压值。数据手册“Figure 67. Initial Flow at Power Up”中要求 VCAP1大于1.1V。
下面的FAQ请参考。