This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC12DJ5200RF: 寄存器0x2c1始终报LINK_ALARM

Part Number: ADC12DJ5200RF
Other Parts Discussed in Thread: LMX2594, LMK04832

您好,

  我正在调试ADC12dj5200这块ADC芯片,10G采样率,采用JMODE1,adc的dclk和sysref分别由lmx2594给出,K=4,sysref = 31.25MHz。LMX2594的Fosc=100MHz,SYNC和sysrefreq均为31.25MHz。这三个频率都由LMK04832输出。

  这三个外设芯片的寄存器配置分别如下:

LMK04832

lmk04832_新板子.txt
Fullscreen
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
R0 (INIT) 0x000090
R0 0x000000
R2 0x000200
R3 0x000306
R4 0x0004D0
R5 0x00055B
R6 0x000600
R12 0x000C51
R13 0x000D04
R256 0x010001
R257 0x01010A
R258 0x010250
R259 0x010344
R260 0x010420
R261 0x010522
R262 0x010600
R263 0x010710
R264 0x010819
R265 0x01090A
XXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXX

LMX2594

sysref_repeat_lmx2594.txt
Fullscreen
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
R112 0x700000
R111 0x6F0000
R110 0x6E0400
R109 0x6D0000
R108 0x6C0000
R107 0x6B0000
R106 0x6A0000
R105 0x690021
R104 0x680000
R103 0x670000
R102 0x660000
R101 0x650011
R100 0x640000
R99 0x630000
R98 0x620000
R97 0x610888
R96 0x600000
R95 0x5F0000
R94 0x5E0000
XXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXX

adc12dj5200

在我完成上述配置后,我回读了FPGA中的jesd204b core的状态,0x3c显示eeee,表明链路正常建立,同时SYNC信号也是一直拉高的,但我回读adc中的寄存器0x208是,它的值是0x64,表明LMFC和sysref没有对齐。同时回读0x2c1,存在link_alarm告警。这个问题我4天前在英文论坛发过帖子,但没有得到任何回复,因为比较紧急,所以又在中文论坛发一次,希望能够得到帮助,谢谢!

x 出现错误。请重试或与管理员联系。