你好,我们现在SPI总线挂载了两个设备,一个是AFE4403,另一个是另一个SPI设备,我发现4403的SPI通讯正常,另一个SPI设备通讯不上,我把4403拆掉后,另一台SPI设备就能正常通讯了,我查数据手册,发现了这个地方,我按照要求的设置也不行,这是我关闭代码的时候的设置。
Disable_AFE44xx_SPI_Read();
AFE44xx_Reg_Write((uint8_t)CONTROL3, 0x0001 | SOMI_TRI |CLKOUT_TRI);
AFE44xx_Reg_Write((uint8_t)CONTROL2, AFE44xx_Current_Register_Settings[35] | DIGOUT_TRISTATE_ENABLE);
Enable_AFE44xx_SPI_Read();