This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1299: 在BIASINV和BIASOUT之间的电阻电容取值

Part Number: ADS1299

您好,我看到ads1299上在BIASINV和BIASOUT之间的电阻电容取值建议为1M和1.5nF。如果我设计64通道,需要8片芯片,所有芯片的BIASIN连接在一起以及所有芯片的BIANINV连接在一起,而仅仅用了一组RC且阻值容值还是1M和1.5nF,是否有问题?谢谢


  • 感谢您对TI产品的关注!
    关于你的咨询,BIASINV和BIASOUT之间的电阻电容 是RC filter,多组芯片连在一起,RC filter也是1Mohm和1.5nF。
    最终的话,在你的设计系统中验证一下比较好。