This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC128D818: 差模输入电压限值疑问

Part Number: ADC128D818


输入差分信号与ADC128D818共地时,根据规格书IN0~IN7 PIN脚耐压为5.3V(电源V+为5.0V);

若输入差分信号与ADC128D818不共地,试问任意一组差分输入端(IN4-IN5、IN6-IN7)之间的差模电压限值是多少?CN1+与CN1-之间接入12V的直流电压,PIN脚是否有损坏风险?

  • 您好,

         差分输入电压最大为(VREF – 3LSb/2)。

        

  • Hi,对于你截图的这部分描述,我的理解是差分输入端(IN4-IN5、IN6-IN7)之间的差模电压推荐在0V~(Vref-3LSb/2)之间,超过Vref-3LSb/2会饱和,但没有提到是否会损坏芯片pin脚,我的问题是:输入与芯片不共地的差模电压时,芯片PIN脚的耐压值是多少?

  • 您好,

          是问共模电压吗?

          就是“根据规格书IN0~IN7 PIN脚耐压为5.3V(电源V+为5.0V)“

         

  • 感谢您的耐心解答。

    不是共模电压,是差分输入与芯片不共地时(即CN1+、CN1-、CN2+、CN2-与A+5V是隔离系统、不共地),差分输入的电压最高可以达到多少V不至于导致芯片pin脚损坏?因为在我的应用中(如下图),当进行产品耐压测试时,差分输入端(IN4-IN5、IN6-IN7)可能存在12V的差模电压(大概1min)。不知道这个电压是否会有损坏芯片的风险?

  • 您好,

          差分输入端(IN4-IN5、IN6-IN7)可能存在12V的差模电压

          ------这就是前面回复中数据手册“8.3.3.2”中要求的电压范围,最大不超过(VREF – 3LSb/2)。

                如果您的设计中存在过压输入,请在外部实行滤波或保护,否则会损坏芯片。