This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS131M08: DRDY中断频率异常

Part Number: ADS131M08


M08使用默认寄存器配置,CLKIN外接8.192Mhz晶,DRDY引脚配置为中断模式。数据采样率默认值应该是4khz。但是用示波器看DRDY引脚,输出的是2Khz的方波。

改变寄存器配置,将clock寄存器的位7置1,OSR取256,寄存器值配置为0XFF86。理论上数据率应该是16K,但是测DRDY引脚是8K.感觉总是一半。

读写寄存器正常,配置FF86,读出来也是FF86,ID寄存器读出0x0801.

请问这种情况是什么原因。