This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS8686S: PSRR数据图的条件

Part Number: ADS8686S


请问这张图中的红色线和蓝色线意思是A、B通道的差异,还是说加了去耦电容和没有加去耦电容的差异,谢谢

  • 感谢您对TI产品的关注!
    关于你的咨询,红色线和蓝色线意思是还是说加了去耦电容和没有加去耦电容的差异。
    这样表示,是为了让2个通道不同的条件,一起看比较清楚。

  • 好的非常感谢。那么想请问一下,实际的给信号的信号源是什么型号呢?因为我用普通信号源和DC源通过注入器加载到VCC上,实际测到的PSRR在1k的时候只有-90dB

  • 你可以看看下面的application report,关于PSRR测试的。

    www.ti.com/.../slaa414a.pdf

  • 您上面提到LDO的PSRR测测试方案,这个是属于模拟输入和模拟输出,用网分可以很好的测量到;对于该产品输入是模拟量,但是输出是数字量,该PSRR测试方案并不适用。其实主要还是想关注贵公司的这个ADC产品PSRR数据的测试方案,想知道模拟输入前端的处理手段或者信号源的情况,以及数字输出FFT的分析方法,谢谢

  • 你试一下下面的测试条件。

    The PSRR (Power Supply Rejection Ratio) measures the noise that propagates to the ADC by varying the power signal to inject noise:

    1. Low frequency (1 kHz) and high frequency (1 MHz) noise signal with 200 mV is applied to the power rail
    2. The input amplitude of the injected noise signal is measured
    3. ADC conversions on a DC voltage is performed; the output amplitude is measured by taking an FFT of the ADC results
    4. The rejection ration is then computed as a ration of the output amplitude over the input amplitude