This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

求教24bit高分辨率位ADC INL DNL测试方案

Other Parts Discussed in Thread: ADS1256

(1)项目对ADC系统的线性度要求比较高,请专家提供一下解决方案,有没有什么参考文献,以及需要哪些实验仪器,以及数据处理方法。

前期我们基于AD7767 SAR类型做过一版,但只是线性度指标1000多ppm,到不到要求,不过也可能是我们测试方法不对,我们只是在-10V~10V范围内,抽取20个点,用电压表测试的,然后数据拟合,看这些点距离拟合曲线的最大距离作为我们的最大偏差,再除以量程我们就认为是我们这个系统的线性度指标。求指点迷津。

(2)再问一个问题,也是我心中的不解。

AD指标有一个动态范围(不是说SFDR),其定义是满量程/RMS噪声,这个指标是衡量什么的?  

SINR也可求出有效位数,那么这个动态范围是不是也和ENOB有关系呢。

为什么动态范围不是用FS除以最小可分辨单元,也就是20*log10(2^ENOB)

(3)关于精度与分辨率再求解释

我的24位AD假如能做到20位,低4位都是噪声,满量程输入10V,那他的分辨率大约10uV,可是我的参考电压都达不到uV 级别,那么在我的精度是mV 级别的情况下,而且我最关心的是测量系统的准确性,那个这个分辨率指标有什么实际的物理意义吗。我怎么个人感觉这个分辨率其实就是表征我这个系统的全部噪声水平啊。

请专家解答。可电话联系 18610346351,诚挚感谢!