This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于ADS8513的问题

Other Parts Discussed in Thread: ADS8513

我在使用ADS8513 芯片进行数据采集。按照手册,选择输入量程为0~4V,但是通过SPI读回的数据,与手册上描述的范围不一致。

请问,0~4V回读数据对应的十六进制是如何计算的?

  • 这可以设置成多种输入模式: The converter can be configured for a variety of input ranges including ± 10V, ± 5V, 0V to 10V, and 0.5V to 4.5V.

    不同模式, 转换结果不同, 但输出线性度应该是没有错的