This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

求解TLC5510 ,如果将REFB与AGND引脚相连,REFT接REFTS,是否就可以将模拟输入电压范围为0V~2.28V的电压转化为数字信号?另外,按照规格书上所说,使用内部基准,0.6V将被转化为8个0的数字信号吗

Other Parts Discussed in Thread: TLC5510

求解TLC5510 ,如果将REFB与AGND引脚相连,REFT接REFTS,是否就可以将模拟输入电压范围为0V~2.28V的电压转化为数字信号?另外,按照规格书上所说,使用内部基准REFB接REFBS引脚相连,REFT接REFTS,0.6V对应8个0的数字信号,2.6V对应8个1的数字信号吗

  • 是否就可以将模拟输入电压范围为0V~2.28V的电压转化为数字信号?

    可以

    使用内部基准REFB接REFBS引脚相连,REFT接REFTS,0.6V对应8个0的数字信号,2.6V对应8个1的数字信号吗

    是的

  • 你好,如果将REFB与AGND引脚相连,REFT接REFTS,将模拟输入电压范围为0V~2.28V的电压转化为数字信号,这个可行的话,规格书的“Analog Input Range – TLC5510 . . . 2 V Full Scale”电压,应该怎么理解,0到2.28范围是不是超量程了,这样的话对芯片会有损坏吗?  谢谢!!!