Other Parts Discussed in Thread: ADS8332
ads8332有数字地和模拟地之分。是否可以用两个独立的电源系统对ads8332分别供模拟电源和数字电源,地与地之间互不相连。
但是产品手册上说AGND和DGND之间的电势差必须小于0.3V。实际上就是逼着我把两个地相连?
我曾经没看到这个小于0.3V的要求,实践了AGND和DGND互不连接,结果也未见异常
是否AGND和DGND可以不连?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: ADS8332
ads8332有数字地和模拟地之分。是否可以用两个独立的电源系统对ads8332分别供模拟电源和数字电源,地与地之间互不相连。
但是产品手册上说AGND和DGND之间的电势差必须小于0.3V。实际上就是逼着我把两个地相连?
我曾经没看到这个小于0.3V的要求,实践了AGND和DGND互不连接,结果也未见异常
是否AGND和DGND可以不连?
通常使用磁珠或者0ohm电阻将AGND和DGND接在一起,实现单点接地,否则二者如果有压差的话会产生浮地。
你的意思是对于这个AD转换器,浮地是不允许的?
其他AD转换器有允许浮地的吗?
为什么AD转换器的数字地和模拟地一定要连接?
DA转换器也是一样一定要数字地和模拟地相连吗?