在选择ADS1253 ADC芯片时,产生了三个疑问:
1:规格书中有提到这样一段话: If the source impedance of the input signal is significant, or if there is passive filtering prior to the ADS1253, a significant portion of the signal can be lost across this external impedance。这是不是意味着在模拟量进入ADC芯片之前,需要添加电压跟随器,而不需要无源RC滤波网络?
2:规格书中提到的通道选择引脚(CHSEL)的说明Digital Input: Used to select analog input channel. This is a Schmitt-Trigger input 。普通的IO口,例如STM32系列处理器的IO口能否直连CHSEL?如不能,该如何解决?
3:ADS1253为差分输入模式。在使用时能否将一端接地,另一端接模拟量输入?
希望能得到工程师们的回复,谢谢!