DAC8831的VDD是不是必须匹配DSP的3.3V供电,不能使用5V的。如果使用5V会不会导致SPI的通信错误?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
这个怎么算,我想产生50K的正弦波,SPI通信,最大能到50兆。
另外根据DSP的输出电平高电平是大于2.7V的,也能满足DAC的高低电平的要求,一定要电平转化吗