请问AFE5805 LVDS输出工作在测试状态下,即EN_RAMP=‘1’时,采用FPGA可以正确解析AFE5805 LVDS输出数据。当 LVDS输出工作在正常模式下,在模拟输入端引入2MHz、100mV正弦信号,用同样的FPGA程序无法正确解析LVDS输出数据,可能是什么原因呢?AFE5805的配置应该注意些什么问题呢?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
没有发现原理图有问题,根据现在的情况,感觉是ADC工作了(内部pattern有效),但前面模拟部分根本没工作(输入信号变化,但数字输出不变),建议做以下测试。
1,请确认模拟供电电压值都正确,只是上电复位,不写任何寄存器,看有无正确数据输出。
2,如果还是没有正确数据输出,参考AFE5808 datasheet page 36 RECOMMENDED POWER-UP SEQUENCING AND RESET TIMING来检查时序,做到一致。
谢谢!