请问ADS1293通过SPI传输心电信号时是在缓存区收集到24位数据然后利用SPI依次传输出去吗?支持FIFO传输方式吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
请问ADS1293通过SPI传输心电信号时是在缓存区收集到24位数据然后利用SPI依次传输出去吗?支持FIFO传输方式吗?
恩,谢谢,请问如果我想把ADS1293采集到的心电信号通过SPI传输到16位或32位的另一个从模式的SPI上,那么我是不是应该在每个通道24位的ECG信号的基础上再传输一个the source of data staus,然后凑齐32位,三个通道再依次传送?那么相当于是传输96位的数据,可以怎么理解吗?还是我可以利用16位从模式的寄存器传输3通道24位的心电信号?