尊敬的TI工程师:
您好!因项目设计需要一款高性能的AD,分辨率为24位,4~8通道,采样速率在每秒2M~5M之间的高速、高精度AD芯片,本人在贵公司的《TI模拟信号链路产品指南》,仔细寻找了也找不到符合要求的,请求贵公司的工程师能不能推荐几款这样的AD芯片。谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
尊敬的TI工程师:
您好!因项目设计需要一款高性能的AD,分辨率为24位,4~8通道,采样速率在每秒2M~5M之间的高速、高精度AD芯片,本人在贵公司的《TI模拟信号链路产品指南》,仔细寻找了也找不到符合要求的,请求贵公司的工程师能不能推荐几款这样的AD芯片。谢谢!
您好,目前24bit的ADC 大部分速率是比较低的。 不知道您是想使用这样一款ADC来设计什么电路? 看看是否真的需要24bit, 2-4M的采样率。
我在我们官网找到了一个ADS1675,可以满足24bit, 2-4M采样率,如果需要多通道,可以使用多路ADS1675。 不知道能否满足你的要求。
非常感谢Jason您的回答,本人打算用这样的ADC来设计电磁接收仪器的前端信号采集部分,基本参数就需要采样率大于1MHz的,分辨率为24位的,我看了下ADS1675,这款ADC是单通道的,目前正准备先评估下这款ADC的性能。
谢谢Seasat您的回答,分辨率高于24bit的也可以,不过采样速率要大于1MHz,是不是目前还没这样的ADC哪?