This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP130SS 控制



目前正在使用DP130芯片,目前根据datasheet操作 I2C 时序,读操作不能够响应,目前需求 操作控制代码

  • 读操作不能够响应, 我看先验证电源,连接(包括焊接),还有时序吧。

  • 你好!

      谢谢你的答复,

      1、对寄存器操作目前是能配置上,可进行读写操作

      2、目前的问题: A.使用DP130  将4路等差输入信号 通过I2C配置 对应到4路等差输出信号,I2C通过软件初始化完成不再对其操作,是否可以??

                                     B.DP130 硬件方面: 将4路等差信号的输入与输出分别接连接器的输入输出;ADDR_EQ=0;EN=1;RSET=1;其余AUX、HPD、CAD均没有连接,是否可以完成 5.4G的数据通信,如果硬件是允许这样操作,软件是如何配置的??

     谢谢

  • 你好!

      谢谢你的答复,

      1、对寄存器操作目前是能配置上,可进行读写操作

      2、目前的问题: A.使用DP130  将4路等差输入信号 通过I2C配置 对应到4路等差输出信号,I2C通过软件初始化完成不再对其操作,是否可以??

                                     B.DP130 硬件方面: 将4路等差信号的输入与输出分别接连接器的输入输出;ADDR_EQ=0;EN=1;RSET=1;其余AUX、HPD、CAD均没有连接,是否可以完成 5.4G的数据通信,如果硬件是允许这样操作,软件是如何配置的??

     谢谢