This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP130硬件 软件如何操作,使用DP130 4路输入直接转到4路输出



  对DP130操作目前的问题: 

          1.使用DP130  将4路等差输入信号 通过I2C配置 对应到4路等差输出信号,I2C通过软件初始化完成不再对其操作,是否可以??

          2.DP130 硬件方面: 将4路等差信号的输入与输出分别接连接器的输入输出;ADDR_EQ=0;EN=1;RSET=1;其余AUX、HPD、CAD均没有连接,是否可以完成 5.4G的数据通信,如果硬件是允许这样操作,软件是如何配置的??

 谢谢