This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

我用STM32F107 SPI方式采集ADC128S022的问题,采到的数据不对,我结合官网提供的M430的例子,没用过M430

Other Parts Discussed in Thread: ADC128S022

我用STM32F107 SPI方式采集ADC128S022的问题,采到的数据不对,我结合官网提供的M430的例子,没用过M430,

#define NUM_OF_RESULTS   8    // Number of temp sensor samples to take
#define ADC_CHANNEL      0    // ADC channel for conversion
#define SCALE_FACTOR     3    // For averaging converted samples
#define ADC12_RATIO    0.805664   // 3300/4096(3300mV ref & 12bit converter, straight binary o/p)
#define ADC_INPUT0        0
#define ADC_INPUT1        1
#define ADC_INPUT2        2
#define ADC_INPUT3        3
#define ADC_INPUT4        4
#define ADC_INPUT5        5
#define ADC_INPUT6        6
#define ADC_INPUT7        7
volatile unsigned char bdata;
unsigned char ADC_Input  = 0x00;  
unsigned char ADC_Cnt  = 0x00;  
unsigned short ADC_Data  = 0x0000;           
unsigned char ADC_Numbytes = 0x00;
unsigned char i ;

void TI_ADC128S022_Init(void)
{
      ADC_Numbytes = 16;
      ADC_Data  = 0;
      AD_CS_DISABLE();
    AD_SCLK_DISABLE();
      Delay(1000);
    AD_CS_ENABLE();
     #if 0
                switch(NUM_OF_RESULTS)  
            {   

            case 0:ADC_Input = ADC_INPUT0;    break;  

            case 1:ADC_Input = ADC_INPUT1;    break;   

            case 2:ADC_Input = ADC_INPUT2;    break;   

            case 3:ADC_Input = ADC_INPUT3;    break;   

            case 4:ADC_Input = ADC_INPUT4;    break;   

            case 5:ADC_Input = ADC_INPUT5;    break;   

            case 6:ADC_Input = ADC_INPUT6;    break;   

            case 7:ADC_Input = ADC_INPUT7;    break;  
            default:   
            break;
            }
            #endif
      ADC_Input = 0xe1;
      for(ADC_Cnt = 0; ADC_Cnt < ADC_Numbytes; ADC_Cnt++)  
    {   
     Delay(1000);    
     AD_SCLK_DISABLE();   
     if (ADC_Cnt<5)
         {
              if(ADC_Input&0x80)  
                {
                    ADC_DOU_ENABLE();
                }
                    else
                        {
                            ADC_DOU_DISABLE();
            }
                        ADC_Input <<= 1;
            }
                        else
                        {
                            ADC_DOU_DISABLE();
            }
                        Delay(1000);
                        AD_SCLK_ENABLE();
                        Delay(1000);
           // if(ADC_Cnt >= 4 )
                    //    {
                    //        ADC_Data <<= 1;  
            
                        //if(ADC_DIN_ENABLE)
                        //    {
                        //          ADC_Data |= 0x0001;
           //   }
                        //    else
                        //    {
                                // ADC_Data &= 0xfffe;
            //  }            
    }
        //    else
        //    {;}
//}
          AD_CS_DISABLE();
      //AD_SCLK_ENABLE();
     // *adc_data   = ADC_Data;
    // return;        
    //    printf("%d\r\n",ADC_Data);         //这儿printf串口输出是4095
}

void TI_ADC128S022_ADC_vout    (void)
{
    uint8_t i;
  static uint16_t results[NUM_OF_RESULTS];       // To store ADC output
  static uint32_t sum_adc_data = 0;              // accumulate and avg adc results
  volatile static float vout;                    // ADC vout
 
  for(i=0; i<8;i++)
  {
    results[i] = SPI_ReadWriteByte(ADC_CHANNEL); // read and store ADC Channel output   
    sum_adc_data += results[i];                  // accumulate result
    Delay(1000);                                  // acquisition time                             
  }
  sum_adc_data >>= SCALE_FACTOR;                 // Average the accumulated sum
  vout = sum_adc_data * ADC12_RATIO;             // ADC vout  
  sum_adc_data = 0;                              // Set Breakpoint here & see measured vout     
         while(1)
        {
        printf("%f\r\n",vout);                   //#define NUM_OF_RESULTS   8    // Number of temp sensor samples to take
#define ADC_CHANNEL      0    // ADC channel for conversion
#define SCALE_FACTOR     3    // For averaging converted samples
#define ADC12_RATIO    0.805664   // 3300/4096(3300mV ref & 12bit converter, straight binary o/p)
#define ADC_INPUT0        0
#define ADC_INPUT1        1
#define ADC_INPUT2        2
#define ADC_INPUT3        3
#define ADC_INPUT4        4
#define ADC_INPUT5        5
#define ADC_INPUT6        6
#define ADC_INPUT7        7
volatile unsigned char bdata;
unsigned char ADC_Input  = 0x00;  
unsigned char ADC_Cnt  = 0x00;  
unsigned short ADC_Data  = 0x0000;           
unsigned char ADC_Numbytes = 0x00;
unsigned char i ;

void TI_ADC128S022_Init(void)
{
      ADC_Numbytes = 16;
      ADC_Data  = 0;
      AD_CS_DISABLE();
    AD_SCLK_DISABLE();
      Delay(1000);
    AD_CS_ENABLE();
     #if 0
                switch(NUM_OF_RESULTS)  
            {   

            case 0:ADC_Input = ADC_INPUT0;    break;  

            case 1:ADC_Input = ADC_INPUT1;    break;   

            case 2:ADC_Input = ADC_INPUT2;    break;   

            case 3:ADC_Input = ADC_INPUT3;    break;   

            case 4:ADC_Input = ADC_INPUT4;    break;   

            case 5:ADC_Input = ADC_INPUT5;    break;   

            case 6:ADC_Input = ADC_INPUT6;    break;   

            case 7:ADC_Input = ADC_INPUT7;    break;  
            default:   
            break;
            }
            #endif
      ADC_Input = 0xe1;
      for(ADC_Cnt = 0; ADC_Cnt < ADC_Numbytes; ADC_Cnt++)  
    {   
     Delay(1000);    
     AD_SCLK_DISABLE();   
     if (ADC_Cnt<5)
         {
              if(ADC_Input&0x80)  
                {
                    ADC_DOU_ENABLE();
                }
                    else
                        {
                            ADC_DOU_DISABLE();
            }
                        ADC_Input <<= 1;
            }
                        else
                        {
                            ADC_DOU_DISABLE();
            }
                        Delay(1000);
                        AD_SCLK_ENABLE();
                        Delay(1000);
           // if(ADC_Cnt >= 4 )
                    //    {
                    //        ADC_Data <<= 1;  
            
                        //if(ADC_DIN_ENABLE)
                        //    {
                        //          ADC_Data |= 0x0001;
           //   }
                        //    else
                        //    {
                                // ADC_Data &= 0xfffe;
            //  }            
    }
        //    else
        //    {;}
//}
          AD_CS_DISABLE();
      //AD_SCLK_ENABLE();
     // *adc_data   = ADC_Data;
    // return;        
    //    printf("%d\r\n",ADC_Data);
}

void TI_ADC128S022_ADC_vout    (void)   
{
    uint8_t i;
  static uint16_t results[NUM_OF_RESULTS];       // To store ADC output
  static uint32_t sum_adc_data = 0;              // accumulate and avg adc results
  volatile static float vout;                    // ADC vout
 
  for(i=0; i<8;i++)
  {
    results[i] = SPI_ReadWriteByte(ADC_CHANNEL); // read and store ADC Channel output   
    sum_adc_data += results[i];                  // accumulate result
    Delay(1000);                                  // acquisition time                             
  }
  sum_adc_data >>= SCALE_FACTOR;                 // Average the accumulated sum
  vout = sum_adc_data * ADC12_RATIO;             // ADC vout  
  sum_adc_data = 0;                              // Set Breakpoint here & see measured vout     
         while(1)
        {
        printf("%f\r\n",vout);                 //数据是205.444321
        Delay(5000000);
        }
}
        Delay(5000000);
        }
}

各位看看,问题出在哪了,急求呀,下面是我的程序,麻烦各位

AD_Sample.zip