This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

cc3200 LaunchPad 的ADC模块功能的实现问题

Other Parts Discussed in Thread: CC3200

1.使用的是TI官方的cc3200 LaunchPad 的开发板

2.芯片是cc3200。

3.软件环境是SDK。

4.ADC这个功能我采用的是参考设计给的例子adc.demo的例子。

5.现在我遇到的问题是:我想通过PIN_58的ADC通道输入模拟量,然后通过Tera Term的串口工具显示转化完成的数字量。但是现在软件我的运行和官网给的结果一样,硬件连接也没有问题。但是就是当我通过杜邦线连接到PIN_58时,显示结果没有变化,也就是说没有读数。

6.我的程序使用的就是直接给的例子的程序没有任何修改,硬件电路就是一个简单的光敏电阻分压电路。

7.是不是要修改程序才能建立软件和硬件的连接呢?