This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请教16位DA芯片电路走线设计

Other Parts Discussed in Thread: DAC8571, DAC7741

我需要从16位DA输出一个差分信号到AD8138芯片。要求模拟信号频率不小于4Mbps,信噪比不小于76dB,信号幅度4.4V。我查了一下手册,Ti的DA支持16位的不多,其中大部分是串行或SPI。如果选这些的话,就得最少64Mbps。而串口或SPI总线是不支持的,因此我选择并口的DA芯片。可供选择芯片有DAC8571DAC7741DAC715PB,其中DAC8571INL最大值为65DAC7741INL最大值为3DAC715PBINL最大值为4,因此初步选择DAC7741PB。但我发现采用DAC7741PB有如下地方需要解决:
     1)参考设计只有单端电压输出,因此怎么产生差分信号输出?有相应参考设计吗?
     2)DA7741PB内部有10V参考电压,信号幅度是4.4V,它外部还需要设置吗,如需设置,电压最大又是多少?
     3)DA7741评估板是不是只有单端输出?如果该芯片不合适的话,哪些芯片合适,请推荐。