我在选型一款24位的ADC芯片,主要原理是通过人工电压注入土壤,通过低通滤波后测量土壤电压。因为周围可能存在工频干扰,因此想使用一款带工频抑制的ADC。
查看ADS131A04的手册,这段话代表有抑制工频干扰的能力吗?另外这款ADC适合测量这类应用的电压吗?或者有更好的推荐吗?


This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我在选型一款24位的ADC芯片,主要原理是通过人工电压注入土壤,通过低通滤波后测量土壤电压。因为周围可能存在工频干扰,因此想使用一款带工频抑制的ADC。
查看ADS131A04的手册,这段话代表有抑制工频干扰的能力吗?另外这款ADC适合测量这类应用的电压吗?或者有更好的推荐吗?


1:ADS131A04具有一定的工频抑制能力,在50Hz和60Hz频率下,ADS131A04的总谐波失真(THD)为-100dB。这意味着该ADC在处理包含50Hz或60Hz基频的信号时,能够有效地抑制这些频率下的谐波失真,从而达到降低工频干扰的目的。
2:该类芯片比较优秀,并且可以应用在土壤中,有客户做过类似的应用,可参考下面的链接
e2e.ti.com/.../ads1115-ads1115