Other Parts Discussed in Thread: ADS1298
您好,该性能演示套件是包含了ADS1x98ECG-FE printed circuit board (PCB)和MMB0(Modular EVM motherboard)模块,MMB0是控制器吗,能具体解释一下什么是模块化EVM主板吗?使用该套件所采集到的脑电信号是原始脑电数据吗?套件中有相关的模拟滤波吗,比如50hz的工频滤波;配套的软件中有数字滤波吗?
您好,该性能演示套件是包含了ADS1x98ECG-FE printed circuit board (PCB)和MMB0(Modular EVM motherboard)模块,MMB0是控制器吗,能具体解释一下什么是模块化EVM主板吗?使用该套件所采集到的脑电信号是原始脑电数据吗?套件中有相关的模拟滤波吗,比如50hz的工频滤波;配套的软件中有数字滤波吗?
您好,
MMB0上面有MCU,安装在PC端的软件通过MMB0配置ADC芯片(4页)。
可以获得原始数据(26页),
有滤波(25页)。
请仔细查阅用户手册介绍。
您好,
也可通过MMB0板上的J14供电,请参考下面帖子讨论的内容。
4.1
Input Short Testing
By default, the EVM powers up with the individual channels to an internal short with a data rate of 500SPS
and a PGA gain of 6. Once the Acquire button is pressed, the Scope Analysis should reflect input
referred VPP values less than 5µVPP;
这段文字想表达的是采集到的一段短路信号的最大值和最小值之差小于5微伏,说明器件是正常的是吗?
那有规定这段信号的长度吗?比如是4000个采样点是符合的,但是数据扩大到8000个采样点最大值和最小值之差会超过5微伏,那么这种情况下器件是正常的还是不正常的呢?