This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ldc1000的测量问题

Other Parts Discussed in Thread: TIDA-00314

尊敬的TI员工:

       您好!

       想向您请教一个问题,LDC1000是什么时候开始测量呢,是初始化完成之后还是只要上电成功就行,或者是需要某些特殊的设置,是否需要在初始化之后延时才会开始测量呢?

  • 有设置,当然先要设置。之后稍加延时

  • LDC1000的开发可以参考这个设计:http://www.ti.com/tool/TIDA-00314

    里面可以下载基于MPS430的C代码。

  • 您好,很谢谢您的回答,现在我可以调通spi,可以读到相应的寄存器的值,除了Proximity Data LSB、Proximity Data MSB、Frequency Counter LSB、Frequency Counter Mid-Byte、Frequency Counter MSB 无法读到值。

    其中我对寄存器的设置是  

    address 0x01       data0x00

    address 0x02       data0x3f

    address 0x03       data0x94

    address 0x04       data0x17

    address 0x05       data0x00

    address 0x0a       data0x04

    address 0x06       data0x50

    address 0x07       data0x14

    address 0x08       data0xc0

    address 0x09       data0x12

    address 0x0b       data0x01

    想请问下您是否是我寄存器设置的顺序或者值有问题,或者是否是超量程了所以没有输出呢?

    谢谢您!