想请教一下TI的工程师:ADS1198内部只有一级放大,且最大只有12倍,真的能采集到ECG/EEG信号吗?如果单芯片真能采集到如此微弱的信号,那么它到底是怎么实现的,需不需要添加别的电路呢?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我也想知道ADS1299 ADS1198这些只有最大24倍放大,参考电压一般2.5V,就算ADC是24位,最小分辨率只有298nV左右,去测量1-10uV的脑电可以的么?不知道楼主弄到其他资料么?
您好,请参考附件,这种信号的测量,前端有个比较复杂的模拟调理电路。
您好,如果内部集成了PGA,信噪比又比较高的话可以直接测量,像测量心率一类的,如果要做比较细致的心电的话,调理电路也是要的。可以参考下我们的评估板,像ADS1299的,资料可以在网上找到。
ADS1299,参考电压2.5V,24位,最小分辨率298nV. 评估板电路我看过了,只是模拟输入前端好像加了滤波,限幅。
举个例子,
心电大概是1-5mV, 24倍放大后是24-120mv,ADC转换过程只是最小分辨率的80536-402684个量级(24mv/298nv,不知道是不是叫量级),那勉强采集画出来的图,还可以。
脑电大概是10-50uV,24倍放大后是240-1200uv,ADC转换过程只是最小分辨率的805-4026个量级,感觉效果就不那么好了。
现在测脑电,信号幅度就更弱了,ADS1299真能测出来吗?
另外如果外端又加模拟电路调理,感觉就不是很好。直接 仪用放大器+高精度低噪声ADC会不会更好?