This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1100: 在官网ADS1100A1IDBVR 当时买了5个,测试时发现两颗异常,三颗正常。烦请工程师帮忙看下,求解!

Part Number: ADS1100


J9端子的第1、2引脚为4-20mA采样电路的输入端,4-20mA信号流经该电路的120R采样电阻,在电阻两端产生电压,ADS1100A1通过采集该电压转换为I2C数字信号,通过ADUM1250隔离后与单片机通信。当J9的1、2端子悬空(空载)时,ADS1100A1的输出信号为满度值,即FFFF,造成测量异常。当J9端子连接信号线时,即使信号线输出电流为0A,ADS1100A1输出数据也能为0(即0000),但当把J9的1、2端子短接(即不通过外部电流输入),则输出还是满度值(FFFF)
麻烦您帮忙看下