我注意到08h寄存器关于CLK_DIV选项的描述有这样一段话,意思是“选择2分频或16分频时,会强制中速模式下低延迟滤波器的OSR为其他速度模式下的值”,我对这个描述不是很理解,从09h寄存器可以看到相同的OSR配置下,低延迟滤波器在中速模式下的OSR值与其他速度模式下不同
08h寄存器中关于CLK_DIV的这段描述是否意味着“只要在08h寄存器中使用了2分频或16分频,并且在07h寄存器中选择中速模式,那么09h寄存器中的OSR值就应该按照非中速模式来理解”,是这样吗?

例如,我是用了2分频,并且使用中速模式和sinx滤波器,OSR设置为01110b时,OSR的值应该是256而不是167,是这样理解吗?