This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
专家们好:我想用DAC8311输出0~5V电压(电流>1mA),有以下疑问:
1.电源5V供电,sync/sclk/din 引脚可否用3.3v驱动(从arm芯片lpc1754输出)。
2.该输出用以给驱动器提供模拟信号,是否需要加额外的跟随电路。
1.电源5V供电,数字输入引脚的有效高电平是不小于0.7*5V,即3.5V,因此3.3V不可以
2. 驱动器是怎么样的驱动器呢?输入的模拟信号需要多大的电流
驱动器是东方马达100w直流电机驱动器,电流大于1mA.
麻烦问一下有没有直接3.3v驱动的da芯片,输出可以达到5V,分辨率至少14位。还要考虑成本问题。
DAC8311的输出是有buffer的,带负载能力可以看datasheet的Figure 8,Figure 10。
有这样的DAC7760,DAC8830等,DAC8830封装简单,但是价格都比较贵,建议你使用原来的,加个I/O总线电平转换器就可以用了
谢谢!