This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC7731E输出波形尖峰很大

Other Parts Discussed in Thread: DAC7731

用DAC7731E做模拟量输出,输入固定码值时,输出正常,(9000对应1.25V);当输入为变化值时(由FPGA解码AD7176送往DAC7731E,采样率(1/72us),采完立即发送到DAC7731E),码值在7A00到8500之间,输出有时出现2V尖峰值,正负都有,正向较多,建立时间2us,之后恢复正常。后端加一阶低通滤波之后(截止频率36K),尖峰脉冲有所下降,大概在0.5V,左右。模拟电源+/-12V,数字电源3.3V。,通过串口发上来的AD7176采集的数据,没有问题。请问这尖峰脉冲是怎么造成的。