Other Parts Discussed in Thread: DAC8830, ADS127L21
我最近在做一个设计,需要用到两路DAC,我之前使用过DAC8830,它的噪声性能非常好,为了节省一片DAC器件,这次设计选用了DAC82002做双路输出。
但测试中发现DAC82002的输出噪声,比我的输入基准噪声高了一个数量级.
我最初以为是PCB布线问题,因为我的验证兼容了DAC82002和两片DAC8830两种方案,于是我把DAC芯片换成了DAC8830再次测试,发现噪声指标正常了,与输入基准相当。
测试使用的是ADS127L21这款24位ADC,时钟16M,OSR=160000,输出速率50sps,然后软件附加了一次sinc滤波,输出速率降低到5sps,测量电路经过验证,输入短路时波动小于1LSB。用这个测试电路测量DAC的基准,基准使用的是LM399,输出经过了<10Hz的低通滤波,所以测量结果显示其噪声在0.1ppmRMS。但当测试由这个基准驱动的DAC82002时,输出电压的噪声超过1ppmRMS,而换用DAC8830则正常,大约0.1ppmRMS。
两种DAC的REF输入都是通过LM399输出端分压并缓冲,芯片引脚处使用10uF+1nF陶瓷电容退耦,接地方式也是一样的(虽然DAC8830有两个接地引脚,但实际上它们在芯片下方是接在一起的),也就是说实际上两者在外围电路和PCB布局方面都没有区别。但我实在想不通为何两者的输出噪声相差如此之大,难道说DAC82002的内部电路与传统的R2R-DAC有什么区别,从而不适合作为高稳定度直流输出吗?