This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

新人求ads7953问题

对10路信号采样         控制开启通道顺序已达到要求采样率      顺序为 400k  200k 400k 100k 400k 200k 400k 6.6k 400k 200k ......

  那么可以得到每次采样间隔1.25us       我该怎么保证每次采样间隔1.25us,与sclk cs有关吗?

序号

类型

幅值

频率

通道数

采样率

1

方波

6V

20kHz

1

400kHz

2

正弦

±8V

10kHz

1

200kHz

3

脉冲

±10V

100Hz

1

100kHz

4

直流

24V

 

2

6.6kHz

5

正弦

6V

100Hz

5

6.6kHz