Other Parts Discussed in Thread: ADS1274
请问ADS1274能够输入单端信号吗?怎么输入单端信号?单端信号的输入范围是多少?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
如果我的输入信号是一个单端的+/-10v的一个单端信号,那么我是不是需要先把+/-10V的信号转换为0到5V,然后我的AINN或者AINP应该接多少V的电压?
AINN接2.5V,AINP输入0-5V即可,这样差分信号的范围为-2.5V - +2.5V
我们现在拿到了ADS1274的EVM板,但是不知道怎么用,能打电话指导一下吗?是不是有什么上位机软件?TEL 13590195718
请下载ADCPro™ 模数转换器评估软件和ADS1x7xEVM User's Guide,上面有Quick Start Guide
Carter Liu ,您能不能给我打个电话,我们在ADS1274的EVM板的使用上还有问题,能不能电话给我指导写,谢谢!!!13590195718
你可以发邮件到ti-china@ti.com,写清楚您遇到的问题,我们这边会给您联系。