This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1256: 在使用ADS1256的时候经常会出现读取出来的值异常

Part Number: ADS1256


ADS1256的时候经常会出现读取出来的值异常,原来用的是16BIT的adc,现在要用24Bit的.可以帮忙分析一下是什么问题吗?有工程师对接一下吗?

  • 产品用在锂电池充电后端

  • 您好

    首先,我们得确保你的硬件连接是正确的。ADS1256的电源、地线、参考电压等都需要仔细检查,确保它们连接稳固且符合规格。

    接下来,我们得看看软件编程方面。ADS1256的初始化设置、读取方式等都需要确保无误。如果你之前使用的是16位ADC,那么可能有些编程习惯需要调整来适应24位ADC的读取方式。

    另外,信号干扰也是一个常见的问题。锂电池充电时可能会产生一些电磁干扰或电源噪声,这些都可能影响ADC的读取结果。你可以尝试添加一些滤波电路或使用更稳定的电源来减少这些干扰。