Other Parts Discussed in Thread: ADS7818, TXB0104, ADS7812, ADS7835, ADS7834
ADS7818为5V供电,数字接口(SPI)能否直接连接到3.3-only的DSP或者FPGA?
该芯片应用范围如何?是否大量供货?谢谢专家。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
ADS7818的逻辑输入高判决电平是3V,逻辑输入低判决电平是0.8V;输出高电平大于3.5V。
所以3.3V的DSP或者FPGA输入信号的ADS7818,只要保证高电平高于3V,就可以正常输入;但是需要注意对应的DSP或者FPGA能否接受3.5V~5V的电平信号。
您可以使用电平转换芯片TXB0104来实现逻辑电平转换,TXB0104价格也便宜。
ADS7818主要应用在低功耗系统和通用信号采集系统中。可以大量供货。
谢谢
可以用,这个芯片是工业级的芯片,低功耗只是它的一个特色,并不指它只能用于低功耗产品中。高电压、大电流下可靠性通常由您的隔离可靠性和电磁兼容设计来决定,电压多高,电流多大?是不是通过PT/CT进行隔离采样?
另外,如果采样直流电压,需要这么高采样率吗?12位的精度够不够?
12位的精度足够了,目前是采样直流,以后也有可能采样工频信号,我们的实际采样速率在10kHz,实际使用没有超过50kSPS,这个速度确实有点儿浪费了,不过考虑价格也没有找到慢一点更便宜的芯片了。
此外希望输入范围大一点,ADS7818范围是5V,ADS7834范围2.5V,ADS7835范围为+-2.5,我希望范围大一点,而且不需要双极性输入,所以ADS7818合适一点,此外ADS7812输入范围更大一点,速度40kSPS应该也够了,但是价格贵太多,使用起来也麻烦很多,总体来讲,ADS7818最合适了,不知道还有没有更好的推荐。
刚刚在面包板上评估过没有问题,已经准备使用了。