This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1256测量范围

Other Parts Discussed in Thread: ADS1256, INA128, ADS1294, ADS1262

请问,

1.假如ADS1256的VrefP接了+2.5,VerfN接了0,ACOM接地,前端测量经过INA128输出的单路电压(此电压对于模拟地有正负),我把,INA128的Vout和ADS1256的AIN0,INA128的模拟地和ADS1256的AIN1相接,配置为差分模式,那么ADS1256前面的接法可以测量吗?

2.假如ADS1256的VrefP接了+2.5,VerfN接了-2.5V,ACOM接地前端测量经过INA128输出的单路电压(此电压对于模拟地有正负),我把,INA128的Vout和ADS1256的AIN0,INA128的模拟地和ADS1256的AIN1相接,配置为差分模式,那么ADS1256前面的接法可以测量吗?

3.

数据手册这里写到,绝对输入只能是正电压,是值AINO-AIN7只能是输入正电信号吗?但是我的INA128的Vout会出现负电压(相对于模拟地)。那怎么办?

举例子:Vout= - 0.5V,那测量值应该是-0.5V-0V吗?


我主要想是测量生物电(脑电,心电,肌电之类)

以上哪一个才能测出前端单路电压(对于模拟地有正负变化的)?请各位和TI工程师解答一下。谢谢!