This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
RT,望前辈知指导谢谢
PGA设置为16,测量范围为±0.256V,1mv的电压是没有问题的。不过为了保证精度,建议前端加放大电路
谢谢回复
我还有个问题,刚刚实际测试发现采集1.05V电压时,万用表读数1.051V,adc采集计算后为1.0505V
采集另一个电压时万用表读数1.537V,而ADC为1.53325V,这是怎么回事,这是我万用表的问题吗
这个不好说,你再找个万用表试试,或者找个稳定的基准测试一下吧
请问下有什么电压基准芯片推荐吗,电压1~2V之间,能精确1mv的
谢谢你的解答
这个范围精度最高的就是LM4132A-1.8了,0.05%精度,勉强能精确到1mV
很感谢您的解答,对我很有帮助