使用了OPA350作为参考电压,但是在实验室中暂时无OPA350,实验室可替代产品有OPA335。比较了一下他们的几个参数,如下所示:
能否用OPA335代替OPA350呢?个人觉的OPA335比OPA350更好。做为缓冲时,是否主要看压摆率指标?希望大家能指点指点菜鸟。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
这个要看数据手册的描述了,如果有unity-gain stable的相关说明,那就是单位增益稳定的
当ADS1256的内部BUFFER打开时,datasheet中ELECTRICAL CHARACTERISTICS表格中,有说明:当打开内部BUFFER时,Absolute input voltage的最大值为(AVDD − 2.0),当AVDD为5V时,单端输入模拟量电压值在0~3V之间。
现传感器电压为-10V~10V,通过AIA电路使信号幅值满足0-5V。而当内部BUFFER打开时,单端输入电压范围为0~3V,而与信号输入幅值矛盾。
我的问题如下: 一:能否在ADC单端输入前,加一级单位增益电路BUFFER替代ADS1256内部BUFFER,增大ADS1256输入阻抗,而同时使输入电压范围处于0~5V之间;此时外部BUFFER的效果是否能代替内部BUFFER的作用?
二:给ADS1256供电的电压芯片是选用TI的TPS7101,其输出电流最大值为150mA;给ADS1256(15mA),四个OPA2333供电,不了解OPA2333的工作电压,这个TPS7101能否带动这些负载呢?
1.我认为是可以的。内部buffer由于不是rail to rail的buffer,所以有个输入范围限制,如果使用外部buffer也要注意这个问题;
2.OPA2333是微功耗运放,其单通道静态电流只有17uA,四片合计4*2*17uA.如果OPA2333所带负载不重,TPS7101毫无压力