你好,
我使用TLV2543做AD采集,但是发现基准电压一直被拉低.
在电路板上只焊接了TLV2543,供电电源为3.3V,基准使用的为LM4040_2.5。
TLV2543的11个模拟输入口都接地(防止悬空),CS脚接10K上拉,REF+接LM4040_2.5,REF-接地。
出现的现象为刚上电一段时间基准2.5V是稳定的,但是过了一段时间就被拉底了,之后就不能恢复了,除了更换TLV2543。
如下图:
谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.