This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS131E04采样率由1KHz提高到16KHz时出现问题

Other Parts Discussed in Thread: ADS131E04

你好:

       用ADS131E04芯片进行采样时,使用SPI接口进行数据通信,使用1KHz采样率,SPI时钟频率为2.048MHz时,DRDY引脚输出1ms一次,读取的AD采样值正常;

1、将采样率由1KHz提高到16KHz时,把SPI的时钟频率由2.048MHz提高到16.384MHz时,用示波器观察DRDY引脚的输出,发现DRDY输出信号的频率由1ms一次变成4ms一次;

2、再将SPI的时钟频率由2.048MHz改成4.096MHz时,其中采样率也为16KHz,DRDY输出信号的频率变成500ns一次(正常),不知道这是为什么?

猜想:

1、因为ADC芯片的主频为2.048MHz,会不会是SPI时钟频率太高,造成DRDY输出出错,即AD采样出错?

2、会不会因为寄存器配置出错造成上述现象?

3、还是说有其他可能?