首先不是很清楚7883的正方向在那边,默认为带横线那边为正方向的情况下,我们用单片机输出的CS和SCLK信号,其幅值是0-5V,但是一接到7883对应的信号端,CS和SCLK信号幅值就变成0-600mV,外接上拉电阻也不能解决问题;然后按横线端为反方向接,CS和SCLK的信号幅值对了,但是数据输出端烦人幅值友不对了,在4.5-5V之间。买了两家的店的芯片结果都是一样的。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
首先不是很清楚7883的正方向在那边,默认为带横线那边为正方向的情况下,我们用单片机输出的CS和SCLK信号,其幅值是0-5V,但是一接到7883对应的信号端,CS和SCLK信号幅值就变成0-600mV,外接上拉电阻也不能解决问题;然后按横线端为反方向接,CS和SCLK的信号幅值对了,但是数据输出端烦人幅值友不对了,在4.5-5V之间。买了两家的店的芯片结果都是一样的。
这是数据手册上的图,上面也是没说清楚,我的芯片上面有条横线,不知道是不是正方向
横线是在最边上吧?如果在边上,那么横线的左边是1脚,能否把你芯片表面拍个照片看下?
按你这个摆放位置的话,红色正对的上方是1脚,下面是6脚。
我用单片机输出的CS和SCLK信号,其幅值是0-5V,但是一接到7883对应的信号端,CS和SCLK信号幅值就变成0-600mV,外接上拉电阻也不能解决问题。
那很可能是芯片本身问题,有没有换块新的7883试试?是不是代理商购买的?
申请样片试试吧,因为直接输入信号接上就不对,很有可能是芯片本身问题导致