This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS131M08: ADCEnergyMetrologyLibrarySW_1.03里的metrology-fir-table.c系数是如何生成的?

Part Number: ADS131M08

你好,

我用ads131m08做电表相关应用,移植了ADCEnergyMetrologyLibrarySW_1.03库,这个库里面有一个metrology-fir-table.c,这个系数是怎样生成的?

它里面定义的最大采样率是:INT_SAMPLES_PER_10_SECONDS == 80000 && MAINS_NOMINAL_FREQUENCY == 50 && PHASE_SHIFT_FIR_TABLE_ELEMENTS == 256

也就是8K采样,但是我这边现在需要16K采样,

需要:INT_SAMPLES_PER_10_SECONDS == 160000 && MAINS_NOMINAL_FREQUENCY == 50 && PHASE_SHIFT_FIR_TABLE_ELEMENTS == 256以及INT_SAMPLES_PER_10_SECONDS == 160000 && MAINS_NOMINAL_FREQUENCY == 60 && PHASE_SHIFT_FIR_TABLE_ELEMENTS == 256 对应的系数表。