This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于CC2451和CC2640内部集成ADC性能问题

Other Parts Discussed in Thread: CC2541, CC2640

CC2541中开发文档swru191f中有描述
with a decimation rate of 512 using only the 12 MSBs of the digital conversion result
register, the maximum value of 2047 is reached when the analog input (Vconv) is equal to VREF, and
minimum value of –2048 is reached when the analog input is equal to –VREF.
是否可以理解为当12bitADC配置为差分模式的时候,此时MSB位为符号位,记录的为补码格式,所以有效数字位只有11位
配置成单端时,12bit的LSB可以达到vref/4096,此时MSB位为第13位吗,还是说此时无符号位
如果供电电压为3.3V(作为ADC参考电压),单端和差分模式下CC2541和CC2640的最小检测信号能达到多少?是不是根据ENOB来测试,精度可以达到12位吗?
项目急用,谢谢