Part Number: ADS1255
Other Parts Discussed in Thread: ADS1260,
我使用7.68Mhz的晶振,想知道如何使用内部的数字滤波器进行50hz的公频噪声滤波,应该配置哪个寄存器,跟采样率的关系是什么样的?此外ADS1260是下一代的升级款吗,有什么升级的地方,有什么不如1255的地方吗
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
1)根据数据手册“Table 12”,选择支持“ Notch at 50Hz”的DATA RATE,并对照“Table 11”设置寄存器。
Very Low Noise, 24-Bit Analog-to-Digital Converter datasheet (Rev. K) (ti.com.cn)
2)ADS1260是 ADS1255 升级版本。
ADS1260没有 XTAL 输入,相反,ADS1260 有一个内部振荡器,这意味着根本不需要外部 clock。
ADS1260 还具有内部 VREF,因此与使用 ADS1255 相比,这可以降低系统成本。
3) 可以,AINCOM使用方法如下。