请教TI专员:
ADS1255\1256 系列的AD转换器其 参考电压只能是2.5V?不能外加5V(或4.096V)的参考电源?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
请教TI专员:
ADS1255\1256 系列的AD转换器其 参考电压只能是2.5V?不能外加5V(或4.096V)的参考电源?
不对哦。从技术手册来看,
Reference input voltage (VREF) VREF ≡ VREFP − VREFN 0.5 2.5 2.6 V
参考电压规定了是2.5V。。。
我只是犹豫,能不能用高参考电压呢?想核实下。。我 迫切需要高电压工作。。
参考电压最大不能超过2.6V啊,一般都是1/2Vcc电压。