This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Sourcing linear driver:3.3V to 24v 100mA

Looking for a driver chip (or level converter, linear driver), the specifications are as follows: input voltage 3.3V, output voltage 24V, output current minimum 100mA, minimum working frequency 10KHz, working environment temperature: -40-85℃。Please recommend me a PN