Part Number: ADS1260
(1)想实现绝对的负压测量,需要使用差分通道,一个通道选择0V一个通道选择±2.5V的Vin范围,从而实现测量吗?

(2)如手册中AVSS等于-2.5V时,AIN的范围可以到-2.5V,但是这种单端的测量是不行的(如之前回复的),这是为什么呢?
(3)如果差分输入,那么AINP AINN的范围为正负±2.5V,其差值在±2.5V即可实现双极性检测?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: ADS1260
(1)想实现绝对的负压测量,需要使用差分通道,一个通道选择0V一个通道选择±2.5V的Vin范围,从而实现测量吗?

(2)如手册中AVSS等于-2.5V时,AIN的范围可以到-2.5V,但是这种单端的测量是不行的(如之前回复的),这是为什么呢?
(3)如果差分输入,那么AINP AINN的范围为正负±2.5V,其差值在±2.5V即可实现双极性检测?
您好,
0v是电平,具体连接到ADC哪个管脚?
请先参考ADS1260数据手册“图 48”,
对于ADS1260采用差分输入(AINX AINCOM 组成3对差分信号)方式,还是单独输入(5个AINX输入 ,AINCOM做公共端)方式,
输入信号均通过“9.3.1.2 Input Multiplexer”转换成差分输入信号进入PGA,处理后再进入ADC转换,
对于ADC来说输入就是差分信号,其范围在±VREF范围内即可。

如果您想在VIN端输入-2.5V, 当VSS为-2.5V时,满足要求。单端或差分输入方式均可。
ADS126x精密 5 通道和 10 通道 40kSPS 24 位 Δ-Σ ADC datasheet (Rev. C) (ti.com.cn)