This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1220的差分通道切换时间问题

Other Parts Discussed in Thread: ADS1220

1.ADS1220如果使用两路差分(01通道差分,23通道差分)在采集过程中,两个通道需要频繁切换。切换后的稳定时间是多少,需要延时多久比较合适?(TURBO模式、2000SPS,、内部基准、内部时钟)。

2.同上,两个差分通道01通道配置为:禁止PGA,单倍增益。通道23使用PGA,128倍增益,这样的通道切换需要多久的稳定时间。

3.差分01通道进行采集(正常模式、1000SPS,、内部基准、内部时钟)。采集完成后断电10S,10秒后,重新上电,发送复位指令,配置ADS1220参数之后,需要延时多久,才能稳定采集。

下面是实测的数据,感觉不对,但是又解决不了,希望能够得到帮助。

1和2测试结果:从通道01(禁止PGA\单倍增益)切换到通道23(使能PGA\128倍增益),需要延时3ms,小于3ms会采集到不稳定的点。

                       从通道23(使能PGA\128倍增益)切换到通道01(禁止PGA\单倍增益),需要延时小于1ms,采集稳定。

                       当改变23通道的配置参数,与01通道相同(禁止PGA\128倍增益),此时通道的切换延时均小于1ms,数据稳定。

3测试结果:先开启ADS1220的数字供电和模拟供电,配置ADS1220参数之后,延时30ms之后,信号采集稳定,否则前面采集到的点,就不准确。(使用示波器                       测试,确定在ADS1220参数配置之前,01通道的输入信号已经稳定)。

上述测试的问题究竟出在哪里,希望有达人能够提供一个思路。