This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM98640噪声问题



1、芯片:LM98640

2、采用第三方的评估板,采用的是参考设计,电路板是PCB板

3、软件环境:FPGA ISE  XILINX  

我现在自己做的PCB电路板,用来处理CCD数据。这块电路板上主要的芯片是LM98640,Virtex5_FF1136_LX50T 和TLK2711。LM98640中的自校图形可以放出来,通过地检软件显示没有问题,每一列的值都一样,无噪声现象。

LM98640用的是手册中提供的电路结构。LM9860的主时钟20MHz。

现在的状态时,LM98604的输入端OS-信号悬空,通过示波器可以看到OS-信号端有一个50mv的40Mhz的周期信号,信号的变化情况与SAMPLE和CLAMP位置吻合。通过我们自己地检软件观测信号值一列大,一列小,或者两列大,两列小。并且每列信号的值的平均误差不太一样,特别是采样模式用的不同时。在SAMPLE模式下,误差码制大约在6个左右,同样条件切换到CDS模式误差码制大约在20个左右。这个噪声和手册不符啊。我们现在的测试情况其实就是在测试LM98640的躁底,手册上是1.8lsb,但是实测最后的情况是6lsb,且出现深浅不一的条纹图案。