各位专家,大家好,我在使用THS1206时候有两个问题,麻烦您帮我解答一下:
1、在test mode下,我把CR0中的bit8和bit9设置为0、1时,即此时THS1206的输出应该是800H,但是我实测的数据是805H或807H或809等,请问这正常吗?
2、THS1206的datasheet中第6页中表格“TIMING SPECIFICATION OF THE SINGLE CONVERSION MODE”中的tc[Clock cycle of the internal clock oscillator]和第18页中的图26中的CONV_CLK的周期tc是同一个东西吗?