This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS7223: 内部REF1,2与CHx的对应关系

Part Number: ADS7223

在手册中只看到设置REFCM寄存器时,可以将CMx设置为REF1或2。但是没有找到REFDAC1,2与CHAX、CHBx的对应关系。

请问:

1. pseudo模式下,REFDAC1,2的作用除了给CMx,还有给CHAX、CHBx提供参考电压的作用吗?

2. 若有,REFDAC1,2与CHAx、CHBx的对应关系是什么?默认值是什么?如何设置?

3. pseudo模式下,A,B通道均需使用,通过设置REFCM寄存器可以将REFDAC1同时作为CMA和CMB的值。那么能否只用REFDAC1作为CHAx、CHBx的参考电压。此时REFIO2能否悬空,即省略REFIO2-AGND之间的22uF电容?

  • 您好,

         请参考数据手册“Figure 29” ,REFIOX是直接给ADC作为参考电压的。   

          REFDAC1,2 对内部参考电压编程输出,作为REFIOX的电压源。

        请参考数据手册 “Table 2” , Pseudo模式下,ADC-可选择REFIOX。

         因此, 若REFDAC1同时作为CMA和CMB的值, 建议使用REFDAC2作为ADC的参考电压。